Intelduopower (Customer) asked a question.
Hello,
this is the error I am getting below. Codesys running on any other system allows for more than 5 bytes. I would like to know what other limitations this plc has.
------ Build started: Application: Device.Application -------
Typify code...
[ERROR] P622: NVL [Device: PLC Logic: Application]: Network variables: Maximum list size reached. Only 5 bytes are allowed.
Compile complete -- 1 errors, 0 warnings
This is the errors I am getting below for the symbol configuration.
------ Build started: Application: Device.Application -------
Typify code...
[ERROR] iecvaraccess, 4.5.0.0 (system): FB_Exit [IecVarAccess]: C0046: Identifier 'IecVarAccUnregisterInstance' not defined
[ERROR] iecvaraccess, 4.5.0.0 (system): FB_Exit [IecVarAccess]: C0035: Program name, function or function block instance expected instead of 'IecVarAccUnregisterInstance'
[ERROR] iecvaraccess, 4.5.0.0 (system): Initialize [IecVarAccess]: C0032: Cannot convert type 'Unknown type: 'IecVarAccRegisterInstance3(_IIecVarAccess3, ADR(result))'' to type 'POINTER TO BYTE'
[ERROR] iecvaraccess, 4.5.0.0 (system): Initialize [IecVarAccess]: C0046: Identifier 'IecVarAccRegisterInstance3' not defined
[ERROR] iecvaraccess, 4.5.0.0 (system): Initialize [IecVarAccess]: C0035: Program name, function or function block instance expected instead of 'IecVarAccRegisterInstance3'
Compile complete -- 5 errors, 0 warnings
This looks to be an errata. Please refer to the updated Documentation Website for details and resolution plan.
https://docs.codesys-p2cds622.com/en/latest/Errata/netvars.html
If there is any further information/clarification needed, please let us know.