YOYO (Customer) asked a question.
i'm using click plus plc c2-03cpu with slot module c2-14d2 to control an ac motor from teknic. i'm able to control the motor via frequency command. I want to get the feedback (torque) from motor but the motor can send only a pwm signal
then i should to convert pwm signal to torque measurement . i cannot find how to read it as high speed input (tried frequency measurement and high speed count but don't work )
any suggestions ?
Excellent post RogerRR, I've attached a project and tested it with a signal generator. The math is written out "long-handed" on purpose so that the operations can be understood. But the constants could be optimized for faster scan performance.
PWM_Input_and_Scaling