Blish (Customer) asked a question.

How can I send custom function codes over MODBUS RTU to a server

Hello, I'm working with the Click PLC connected to a PZEM-004T power monitor. I'm able to read the parameters with the Modbus Receive block using function code 4. The problem I'm having is my requirement to reset the energy counters. This requires me to send function code 0x42 to the unit. How can I do this? It appears the only function codes available are 1-4, and 5,6,15,16.


  • ADC Community_02 (Automationdirect.com)

    Unfortunately, there is no way to send function code 0x42 by using the Click plc.

    Selected as Best