Slad (Customer) asked a question.

GS4-4040, EOL1 fault.
Scalar mode.

Hi

How would u interpret this fault:

 

OutFreq: 1.50

OutAmp: 90.30

OutVolt: 20.0

 

Stuck at start up?


    • Slad (Customer)

      Hi,im more into figuring out if the drive faulted at start up, or while running.

  • OkiePC (Customer)

    What is the nature of the driven load? If it requires high starting torque, and your VFD is set up for a normal application, then you might be able to get it to run by adjusting the application settings of the drive. If the load is a normal one, then something is wrong with the load or the motor for it to call for 90 amps from your 60 amp drive.