Grant PLC 1 (Customer) asked a question.

Has anyone had this error occur when trying to work with the Panel Manager in C-More Programming Software? DataBase Initialization Failed....

Error messageimageimageAll tags are gone in the tagname database and I can no longer add tags or see system tags. I can however open the project on another computer and it works fine, thankfully.


  • ADC Community_02 (Automationdirect.com)

    1.) What version of C-more software are you using?

    2.) Have you tried uninstall and reinstall of the software?

    3.) Try right clicking on the C-more programming icon -> select run as administrator. Does the issue persist?

  • Grant PLC 1 (Customer)

    Thanks for the reply,

    Answers to your questions:

    1) V 6.76

    2) Yes, multiple times

    3) Tried that too.

  • ADC Community_02 (Automationdirect.com)

    Forgot to ask in last post:

    1.) What version of Windows Operating is running on your PC showing this issue?

  • ADC Community_02 (Automationdirect.com)

    1.) Did the project ever work on this PC? 

    2.) How did you acquire the project? Read from Panel, another PC, or developed on this PC?

    3.) When Reinstalling the software, have you Uninstalled, Deleted all installation Files and Folders, rebooted and then installed and then rebooted?  This would make sure there are no broken components left behind.

  • Grant PLC 1 (Customer)

    Yes it worked for months with no issues. I wrote the program on this PC. I'm not sure what happened as it was not during a Windows Update. The project will work on other PC's without issues. I'll probably change PC's and move on, was just curious if anyone else had seen this issue and could apply a quick fix. I will try to uninstall and make sure to delete all installation files/folders one more time. Thanks for your help.

  • ADC Community_02 (Automationdirect.com)

    Take a look at the anti-virus software on that specific PC. This can possibly cause the issue you are seeing.