SeanWoold (Customer) asked a question.
Controlling an analog output module with a sequencer.
I have a 0-10v pressure regulator and I'm trying to set up a sequence of pressures for a test with a P1000 and a P1-04DAL-2 analog output module. It seems like the sequencer is the way to go with this, but it isn't clear to me how you can get the sequencer to feed analog values to the output module. Has anyone done this? Is there a better route that I'm not seeing?
Just write a new value at anew step.
Where though? The only way I have figured out how to do it is to use the step numbers as the input for a non-linear scaler which is really weird. Is there a place to enter values directly in the sequencer that I'm not seeing?
Im not familiar with P1000,use a new step bit to load (MOVE) a new value into the analog out register.