Slad (Customer) asked a question.

DIs control by comms.

Hi

I have Sureservo2,Click plus and Cmore over Modbus TCP,all comms are set up and ok.

Im trying to control digital inputs by comms, the manual sais,all u have to do is set P3.006 to 1 and write to P4.007 (Modbus 401039) whatever combination u need...thats the only thing im not able to get done,..in the Click send instruction im not getting any error,but DIs on the Sure servo2 dont change.

Anyhelp would be greatly appreciated.

Ths.


  • ADC Community_02 (Automationdirect.com)

    Take a look at the attached zip file containing programming example & application note for the Click to SS2. It may help shed some light on controlling DI inputs via software instead of hardware.