JB2020 (Customer) asked a question.
I have a rotary moulder that produces pet food. There is a die roll that is driven by a 7.5 hp motor. Below this die roll is a press roll that is hydraulically pressed up against the die roll. A conveyor belt is driven by running between these rolls. The conveyor belt also runs around several other rollers. One of these rollers is considered a Belt Assist roller and is driven by a 2 hp motor. Some products require the belt assist to run and others don't.
On the products that require the belt assist roller to run...I would like to match the speed of the die roll. There will have to be offsets or some kind of math calculation to calculate the frequency at which it needs to run, because the die roll is approximately 12-14" in diameter and the belt assist roller is only 2-3" in diameter.
With all that said, here is my question....
Is an encoder the way to go with reading the speed of the die roll and then translating that to a frequency value for the belt assist roller? I'm not sure I like this idea because the die roll would have to start running before the belt assist roller.
Or can this be done within the GS20 drives by reading speed and/or frequency of the die roll and and sending the correct frequency to the belt assist roller? I'm thinking this will allow both motors to start simultaneously.
I will over simplify this a bit but when the line is running i have the master drive running in speed control and the slave drive in torque control. I tell the slave to run with we will say 50% torque. I also calculate the theoretical speed I expect the slave motor to be running at based of the speed the master is running and do not let the slave run more than a certain amount over or under that calculated speed. I do that incase the rolls get glazed over and have no grip so it doesn't start slipping and running away.