Javi (Customer) asked a question.

ViewMarq Serial Communication to PLC unsuccesful

I'm trying to get a "ViewMarq" display to respond to an ASCII string I'm sending to it via serial RS232. I connected a PC running "hyper Terminal" in place of the marquee display as I wanted to confirm that the PLC was sending the command and that the content of the command was what I was expecting. I would like to know if this ASCII string is correct and if so, why the ViewMarq doesn't respond to the message. The ViewMarq doesn't do absolutely nothing.ASCII String


  • kewakl (Customer)

    How many characters in that message?

    ViewMarq Help topic VM012 states that the limit is 500

  • Javi (Customer)

    I setup my PLC to send the string command every minute while I troubleshoot my issue. There are three string commands on that picture. My command consist of​ only 87 characters.

  • kewakl (Customer)

    Is your CR ($0D) part of the string, or is it the Terminator code in the PLC comms instruction? -- or both?

     

    Have you tried your string in the Viewmarq software?

  • Javi (Customer)

    The PLC I'm using doesn't have a communication instruction setup interface like the Click, or the Allen Bradley, etc. It is all hard source coding. I have the CR as part of the code I'm using to construct the command string.

    ​

    The string I'm using, I got it from the ViewMarq software.​

    • 20230602_055419