Auto101 (Customer) asked a question.

From Arduino MEGA2560 to P1AM-100

Hi will the P1AM-100 be able to do the same operations as the Arduino MEGA 2560? In other words can i use my development code change the chip selection and upload to the P1AM-100?

 

All my dev was done using a Arduino MEGA and was wondering if I can use your product once I be in production. I would like to reproduce the equivalent of the MEGA operation using P1AM-100.

 

Anny help would be appreciated.

 

Looking forward to your response.

 

Best regards.


  • FACTS_AdamC (AutomationDirect)

    It'll depend how you're using the MEGA 2560 and if you're using any features unique to that chip when compared to the SAMD21 in the P1AM-100. For instance, the P1AM-100 GPIO pins are only 3.3V tolerant compared to the 2560 GPIO that are 5V tolerant.

     

    Could you provide more details on your application?