Ed (Customer) asked a question.
Hello community,
Using a P2000, I need to have a new data log file start every time a user hits the start button. I want a new file, not to just start/stop data logging.
Below is per the Help, but I don't see how I can use these to reset the file per ladder logic. Suggestions would be much appreciated.
Ed
Productivity Help "Data Logger"
-----------------------------------------------------------
Note: A new log file will be generated in the below cases. If a scheduled interval is chosen these cases are still applicable:
1) Stop -> Run (including power up)
2) New Config [New Project] sent to CPU (Run or Stop Mode transfers)
3) Pen drive eject
4) Set Date/Time
5) Scheduled file name change
Try item 4.
Copy
Clock [Hours & Minutes & Seconds] to Clock [Hours & Minutes & Seconds] Set
Set
Initiate_New_Time
Check if this procedure will create a new log file. I do not know if the logger requires a CHANGE of time or just a time set attempt.