Arash (Customer) asked a question.
#include <Arduino.h>
#include <P1AM.h>
#include <SPI.h>
#include <SD.h>
#include <Wire.h>
#include "RTClib.h"
RTC_DS1307 rtc; // create an instance of the RTC library
const int SD_CS_PIN = SDCARD_SS_PIN; // SD card CS pin connected to P1AM slot 1 pin 4
const float VCC = 3.3; // supply voltage of the voltage divider circuit
const float VREF = 5.0; // reference voltage of the P1AM input module
const float R_REF = 1000.0; // reference resistor value for the voltage divider circuit
const float R_0 = 1000.0; // resistance of the PT1000 sensor at 0 degrees Celsius
const float A = 3.9083e-6; // constant A for PT1000 RTD
const float B = -5.775e-7; // constant B for PT1000 RTD
float temperature[4]; // array to store temperature readings
float resistance[4]; // array to store resistance calculations
unsigned long previousMillis = 0; // variable to store the last time a data point was collected
const unsigned long interval = 5000; // interval between data collection in milliseconds
const unsigned long duration = 500000; // duration of data collection in milliseconds
File myFile; // file object for writing to SD card
const char P1_04RTD_CONFIG[] = { 0x40, 0x03, 0x60, 0x03, 0x20, 0x02, 0x80, 0x00 }; // PT1000 configuration
const int SLOT_NUMBER = 1; // slot number where the input module is connected
void setup() {
Serial.begin(9600); // initialize serial communication at 9600 baud
while (!P1.init()) {
; // wait for input module to initialize
}
P1.configureModule(P1_04RTD_CONFIG, SLOT_NUMBER); // configure input module with PT1000 settings for slot 1
pinMode(SD_CS_PIN, OUTPUT); // set SD card CS pin as output
if (!SD.begin(SD_CS_PIN)) { // initialize SD card
Serial.println("SD card initialization failed!");
while (1); // stop program if initialization fails
}
rtc.begin(); // initialize the RTC module
if (!rtc.isrunning()) { // check if RTC module is running
Serial.println("RTC is NOT running!");
}
myFile = SD.open("data.csv", FILE_WRITE); // open file for writing
if (myFile) { // check if file opened successfully
Serial.println("File opened for writing.");
myFile.println("Date,Time,Channel,Temperature"); // write headers to file
} else {
Serial.println("Error opening file for writing!");
}
}
void loop() {
DateTime now = rtc.now(); // get current date and time from RTC module
unsigned long currentMillis = millis(); // get the current time
if (currentMillis - previousMillis >= interval) { // check if interval has elapsed
previousMillis = currentMillis; // update previous time
for (int i = 0; i < 4; i++) {
temperature[i] = P1.readTemperature(1, i + 1); // read temperature from input channel i+1 in slot 1
resistance[i] = (VCC * R_REF * temperature[i]) / (VREF * (VCC - temperature[i])); // calculate resistance using voltage divider circuit equation
myFile.print(millis()); // write current time to file
myFile.print(","); // separate time and temperature with comma
myFile.print(i + 1); // write channel number to file
myFile.print(",");
myFile.println(temperature[i]); // write temperature to file and add newline character
Serial.print("Channel "); // print a label for the temperature reading
Serial.print(i + 1);
Serial.print(": ");
Serial.print(temperature[i]); // print the temperature value
Serial.println(" degrees Celsius"); // print the unit of measurement for temperature
}
}
if (currentMillis >= duration) { // check if duration has elapsed
myFile.close(); // close file when program ends
Serial.println("Data collection complete.");
while (1); // stop program
}
}
Your include is showing RTClib I believe it should be:
Unfortunately, It didnt work!
I just want to report the time and date of the temperature data acquisition and put it in the excel file
You wrote; " I believe that I installed AnalogRTCLib from library."
I would double check that is actually the case, if so, I would try one of the example that come with the library and see if that works. If the library is not actually installed I'd try to install it again.