Jeffln12345 (Customer) asked a question.
I need help to program a analog output to go from 4 to 20 milliamps in a set time that i could change if needed.
I have a gate actuator that i want to open slow and close as fast as the actuator will move. i want to use one digital input for control, power to open and loss of power will close.
I have a click C0-12DRE-1-D
This is an idea but not tested. As a note, I force a value to DS1 as a starting setpoint for the timer. Opening DataView1 on the left hand directory tree allows you to edit this value to whatever you want. I am assuming 4mA (0) is closed and 20mA (100) is open.
Gate Close via analog output