da86 (Customer) asked a question.
I have used click for several years but I have not needed to link two clicks till now. My current application involves sending a alarm bit between the two units so very simple. I have been trying to learn the programing required but some help would be appreciated!
Take a look at the below link it contains a master and slave project examples in the .zip file:
https://community.automationdirect.com/s/article/Example-Program-Click-Read-and-write-values-from-on-plc-to-another-1581014678636
**Edited**
Note: The projects are setup using serial com ports. You will need to go Setup -> System Configuration to select your model CPU and then modify the Receive and Send instructions to use port 1.