Linuxdept (Customer) asked a question.

Click PLC PID instruction to generate a PWM

i was Told that that the PID instruction can be used to generate a PWM signals does anyone have any examples of this, it is used for a teknic clear core Motor CPM-MCVC-3432S-RLS.

thank you all


  • ADC Community_02 (Automationdirect.com)

    If you search PWM in the Click software help file there are a couple of topics that will help get you set up CL246 & CL243.

     

    To control a motor you could also use the high speed PWM function in the Click. That is covered in topic CL293.