AdamE (Customer) asked a question.
Hello,
Just getting back into PLC/Arduino programming 21 years later into my career...I'm looking to use the P1AM to control Linear actuators using the P1-16TR as my relay modules. I'm just not exactly sure how to wire them into the outputs. Can I get a quick explanation or wiring help of how the P1-16TR will work? I will be using either 12 or 24 VDC actuators. I plan to power them with a power supply, but I'm stuck from there. I've made a concept machine with a manual rocker switch, but I'm not sure how it will work with the relay module.
Thanks!
Adam
in a previous response i replied
"I myself would us a P1-15TD2 DC sourding output card, 2 782-2C-24D 2 pole relays, and 2 782-2C-SKT relay sockets. this way you can interlock them to make sure only one is on at a time.
https://www.automationdirect.com/adc/shopping/catalog/programmable_controllers/productivity1000_plcs_(stackable_micro)/dc_i-z-o/p1-15td2
https://www.automationdirect.com/adc/shopping/catalog/relays_-z-_timers/electro-mechanical_relays/782-2c-24d
https://www.automationdirect.com/adc/shopping/catalog/relays_-z-_timers/relay_-a-_timer_sockets/782-2c-skt"
The P1-15TD2 is a DC sourcing output card with 15 outputs. the 782 part numbers are relays, but if you are planning on running multiple linear actuators off the same relays i suggest a 784 4 pole double throw contacts
https://www.automationdirect.com/adc/shopping/catalog/relays_-z-_timers/electro-mechanical_relays/784-4c-24d
https://www.automationdirect.com/adc/shopping/catalog/relays_-z-_timers/relay_-a-_timer_sockets/784-4c-skt-1