JJ123456 (Customer) asked a question.
I have a CLICK C2-03 PLC. It had firmware version 2 something.
I attempted to update the firmware to v3.31.
It got to 100% complete on 2/4 (updating firmware) then froze.
Now it says there is no firmware installed and I need to install it. When I try and install it, I continuously get a PTC-005 error. I spam the button and eventually can get it to try and install again but it always stops at the same point (2/4) and gives me a GUI-022 error.
I have restarted everything.
I am using the same laptop that I have connected to this PLC before and all my other CLICK PLCs. I am connected through USB and have tried multiple cords that work on other CLICK PLCs I have.
My laptop has 25 gb of memory free.
I had a ton of PTC-005 errors and had it fail the firmware update a couple more times (GUI-022) but eventually it updated it with V3.41. Its working now.