ADC_HMI_PE (AutomationDirect) asked a question.
https://www.automationdirect.com/support/software-downloads?itemcode=C-more%20EA9%20Series
New Features
1) Simulator Values are now retentive.
2) Simulator Values are now saved with the project.
Improvements
1) Security Updates
Bug Fixes
Software
1) Web Server not connecting correctly.
2) When the Tag Address is edited from within an existing Object the project sent to the panel is still
requesting the previous address.
3) If the Email Action Body is blank, the panel drops the connection to the mail server.
4) Very large Allen-Bradley L5K/L5X file causes failed to Import.
5) Tag Name Database tag usage not showing correctly for some tags
C-more EA9 Software v6.75 Release