erik.carlsen (Customer) asked a question.
Error is-
"This model does not support this instruction or input instruction is incorrect"
No comparisons I've tried work with any data formats. Tried lots of combinations.
??? Very poor fit for my application without this instruction. All other instructions function, compile, run on the drive fine.
Thanks to anyone that might have some insight on this.
It appears that when using a LD compare instruction with a conditional contact in front of it is causing the compile error. Possible bug with the software but has not been confirmed as of yet.
There is a workaround that if you write the ladder like below with the conditional contact after the LD compare instruction it will compile with no errors. I have reported this to our Drives Product Manager.