ADC_HMI_PE (AutomationDirect) asked a question.
CLICK Software Release 3.40
New Features
- CLICK PLUS C2 series CPUs - Secure Email using TLS
- C0 and C2 series Ethernet capable CPUs - Allow List, allows only configured IP or MAC addresses to communicate to certain PLC ports and protocols.
Improvements
- Termination character option added to Copy Instruction Single, Block, and Fill modes.
- Data Logging Setup added text reminder that the maximum rate is 1 trigger/second.
- PTO Home Instruction Switch Inputs can now define their active level: Normally Open, or Normally Closed.
- Pack Copy Instruction for C0-1x and C2-x CPUs now allows TXT to numeric conversion to include leading or trailing whitespace.
Fixed Bugs
- Search/Replace would not find results with certain XD or YD search ranges.
- ASCII Send Instruction did not function when configured with Termination Characters.
- Find Instruction did not include the PTO Instructions: Home, Velocity, and Position.
- PTO Instructions were incorrectly allowed to be Copy-Pasted from the Main Program into an Interrupt Program.
- When switching quickly between PID Setup and PID Monitor dialogs, software may crash.
- Certain USB to Ethernet Adapters may cause firmware update to fail at 70% complete.
- New error messages when loading project files into CPUs which do not support new features. The product family (C0-x, C0-1x, or C2-x) of the project must now match the connected CPU family.
CLICK Software Release 3.40
Known Issue:
PTC-005 Communication Error when updating firmware from v2.x to v3.40 using v3.40 software.
Work Around:
Use an earlier version, i.e. v3.31 to update the PLC to v3.31 firmware, then use v3.40 software to update to v3.40 firmware.
If I update the firmware version PLC Click Plus from 3.40 to 3.91, will the program be lost or what will happen?
Referring to Click help topic: CL014
Since any project in the memory of the CPU will be erased, the option is given to make a backup of the project file if one is detected.
https://cdn.automationdirect.com/static/helpfiles/click/Click_Help.htm#014.htm?TocPath=Main%2520Menu%257CPLC%2520Menu%257C_____14