R985 (Customer) asked a question.
We've found that the P1000 PLC is a great piece of hardware for distributed control, machine automation, and machine monitoring across our facility. In most cases, each PLC is connected to just a handful of I/O points, so each installation draws relatively little power. Since we have to run network cable to the PLC anyway, it would be great if we could just power the PLC via Power Over Ethernet, rather than finding a local power source at the point of installation.
Does anyone know of a piece of hardware that can connect inline with the P1000's ethernet cable and supply 24vdc to the PLC via POE?
Thanks!
Matthew
https://www.trendnet.com/products/industrial/Industrial-Gigabit-UPoE-Splitter-TI-SG104
I have not used that device, but have used some from Tycon that were not din rail mountable and they worked well to split POE for other hardware (not a P1000)