BCMaint (Customer) asked a question.
Using Productivity 1000 with P1-4ADL2DAL-1. What we're trying to do is control vacuum with a 4-20ma control valve. My set vacuum is 25inHG. The vacuum sensor isn't installed in the system yet, but if I pull a slight vacuum, the output just bounces between 0 and 4095. I have tried the auto tune by pulling a slight vacuum (10inHG) and holding it forever, nothing changes in the auto tune. It's not even showing the 10inHG on the PV plot. My variables are in min/max=0/30 out min/max=0/4095. The loop is in auto except for autotune. I've never used the 1000 PID before. I assumed the analog output would slowly drop as the PV got closer to the setpoint.
Thanks for replying. I think I have it figured out. I was being impatient with the auto tune, so I watched the video series on PID and manually tuned it. It seems to be working now. I'll try the autotune again once the system is put together. Thanks again.