Ivgeny (Customer) asked a question.
Hello,
Need help with troubleshoot my connection of CLICK (Ethernet) C0-11DD2E-D with Weintek PLC.
According to instructions, everything is pretty straight forward but the HMI says that "Device no response". I made an IP settings in both sides successfully, checked ping OK
Did I missed something in the configuration ?
all my ports in PLC are busy. I connected online with my PC via port-2 (rs232). PLC connected to VFD via port-3 modbus, and it supose to be connected to HMI via port-1 (Ethernet)
Thanks
Release notes from CLICK Programming Software:
Improvement:
Whereas your 3rd party device is a PLC rather than HMI, the statement is still relevant. Modbus TCP on port 502 should be used for communication between the two devices.