shanem717 (Customer) asked a question.
I am needing to monitor a pressure transmitter 0-300 psi 4-20mA output into click plc with a C0-04AD-1 module and activate a output to a relay if the pressure reaches 250 psi or above, can some one help write a program that will do this, I am also transmitting the pressure to a hmi, thats why i didnt use a pressure switch instead
Hi @shanem717 (Customer)
Can you tell us what CPU model you are using?
What have you got so far with the program? Can you attach a copy?
The Click PLC has a scaling feature when you set up the analog card.
The program would just be a comparison.
Here is a series on the Click PLC that you can use for reference.
https://accautomation.ca/series/click-plc/
I hope this helps you out.
Regards,
Garry
ACC Automation
https://accautomation.ca/
Click Analgo Scaling