Betz (Customer) asked a question.

Using a P1AM-100 to pull data from an omron CP1H-XA40DR-A

I want to pull the data from the Omron PLC and bring it to the P1AM-100, them send over the Ethernet to an IP address. I already do the data send to the IP address using the P1AM, I need to be able to add more data that I gather from the Omron PLC to add to it. Is this data grab possible from the Omron PLC?