kckdistilling (Customer) asked a question.

Unable to ad a C0-08TR output module to a C0-12ARE-2-D. PLC error "[102]-System Config Error"

I recently added a C0-08TR output module to an existing click C0-12ARE-2-D FW 2.51 system(no other modules installed prior). First I connected to the PLC and downloaded the current project from it. I can see the new module in the software under the setup>System Configuration and have set the power budget correctly and hit OK. Next I wrote the project back to the PLC and tried to run it but I keep getting PLC error "[102]-System Config Error". What step am I missing? I can't find an application note or user manual heading about adding modules to existing systems. Anyone know of a tech note, etc that can help?


  • kckdistilling (Customer)

    Fixed it. Did a reset to factory default and reloaded the project. Error gone.

    Selected as Best
  • ADC Community_02 (Automationdirect.com)

    **Edited**

     

    Check the label on the side of the module and make sure the part number says C0-08TR then check system configuration and make sure C0-08TR is the module in I/O slot 1. The system thinks the module you have in your system configuration does not match the installed module. Below image referenced from help topic CL066.

    image

    Expand Post
  • kckdistilling (Customer)

    Fixed it. Did a reset to factory default and reloaded the project. Error gone.

    Selected as Best