Hughjack (Customer) asked a question.

How Can I Access the Registers in the Productivity P2-RS Slave Units for the Connected Modules without the P2-550 PLC

I have two P2-RS and connected modules, but the P2-550 is on indefinite backorder. Does anyone know how to indirectly access the module registers of slave units without the P2-550. I was hoping to pull in the signals to another PLC and access through the MODBUS connection. However, tech support indicated that the addresses could not be accessed without the P2-550.

 

Is there a hack or a manual identifying the MODBUS addresses corresponding to the I/O, or some way to access these registers outside the P2-550 platform?

 

Also, does anyone know where I could find a loaner or another source for the P2-550 other than Automation Direct?