you can find the project properties under the file menu and it will be under the print button, once the pop up screen pops up, press calculate on right side of pop up to display current usage
I haven't seen anyone yet ever have to consider memory on a Productivity CPU. Only people who came from older generation PLCs seem to even think about it. I do love that even the P1k got the same memory as the bigger Productivity models 👍
The base memory usage seems to be around 6% for necessary system stuff. But even my largest program still only gets up to 8% memory usage. I would be very surprised to see someone over 15% used even with multiple, large string arrays..
Please reference help topic P032. Go to file-> project properties -> click on calculate.
you can find the project properties under the file menu and it will be under the print button, once the pop up screen pops up, press calculate on right side of pop up to display current usage
I haven't seen anyone yet ever have to consider memory on a Productivity CPU. Only people who came from older generation PLCs seem to even think about it. I do love that even the P1k got the same memory as the bigger Productivity models 👍
The base memory usage seems to be around 6% for necessary system stuff. But even my largest program still only gets up to 8% memory usage. I would be very surprised to see someone over 15% used even with multiple, large string arrays..
Thank you :-)
I do agree that the memory capacity is "Vast" in conventional PLC terms. (A good thing).
I shall immediately try to fill it! :-)