JB2020 (Customer) asked a question.

Reset Faults with GS Write in Productivity

Hello,

In the GS Write instruction in Productivity Suite, there is a Fault Reset parameter that has a parameter number CTL.03. It is the same number on both GS4 and GS20 drives. Do I need to write a 1 to this location to reset faults on these drives? And do I need to immediately write a 0 back in its place to make sure it doesn't hold the reset? Hope this makes sense!


  • ADC_DriveMotorsLSPLC_PM (AutomationDirect)

    We recommend to set value of 1 for at least 2 or 3 cycles of the GSW instruction (depends on the Poll time setting) and then change it back to 0.

  • JB2020 (Customer)

    Thank You! This should help me out!