Cap (Customer) asked a question.

Bug in V6.70

I've had this happen a few times, and today was the day I mention it.

I have an EA9 running V6.70 Software. Many Screens all retrieved by a Multi Button Screen Change Object. This 25 Button Object is placed at the Lower Right of all the Screens. It's an Object of Each Screen.

This Morning I went from Home Screen (1) to Screen 2. The Screen Change Button did not show up. It's an Object in each screen. I was unable to get out of screen two. In the Past when this has happened, I just Power Cycle the Screen, to get back control of it. Today I was not in a hurry, so I let the 10 Minute Timer in the PLC time out and Revert back to Screen 1. It did that.

Then I went back to Screen 2, and the Screen Change Button Group was there.. I was able to switch back to any other screen I wanted..

 

Is this a 6.70 thing?.. Will 6.71 Fix this.. Or is the not been noticed before..

 

Cap


  • kewakl (Customer)

    IF you have any visibility tags assigned to any screen change objects, 6.72 may have resolution.

     

    1. Bug Fixes
    2. Software
    3. 1) Fixed Microsoft .NET error in software.
    4. 2) Fixed issue where changing Tag Name data type in the Property List for a Tag Name used in a comparison, such as Visibility or Event
    5. Trigger broke the comparison so that the comparison was never true.

     

    Expand Post
  • ADC_HMI_PE (AutomationDirect)

    Are you operating in Portrait mode by chance?

  • Cap (Customer)

    Nope..

     

    Landscape..

     

    Cap