Todd Dice (Customer) asked a question.
So, what does "lock" mean?
Edit: on another note, I wish the indicator went above 255 states (32-bit would have been handy) AND list them with a state number independent of trigger value. In this case, my trigger values start at 809775425, the next at 80977544, etc. so the "simulate" doesn't really work well in this application.

Hi @Todd Dice (Customer),
Lock - Select this checkbox to prevent the object's position or size from being changed accidentally.
This can be seen and controlled on the ...
Object Layer List.
editing
a. The Object Layer List also allows you to access individual objects in a group without
ungrouping and has additional lists for hidden, locked, or overlapping objects Bug Fix
Regards,
Garry
https://accautomation.ca/series/c-more-hmi-series-panel/