kewakl (Customer) asked a question.
forum feature suggestion
Can the forum software make it so that the 'Post Likes' be a HOVER instead of a CLICKED link, so that It does NOT have to be 'dismissed.'

kewakl (Customer) asked a question.
Can the forum software make it so that the 'Post Likes' be a HOVER instead of a CLICKED link, so that It does NOT have to be 'dismissed.'
Copyright © 1999-2023 AutomationDirect. ALL RIGHTS RESERVED
Are you referencing the like button on a thread?
>Are you referencing the like button on a thread?
yes.
For the 'nn LIKEs' popup, I have to locate my mouse cursor and then move it to the [X] to dismiss the popup.
If the 'nn LIKEs' were a mouseover and automatically dismissed (as the User info popup currently works,) that would be good.
[EDIT added nn and s to LIKE
Like popup? When I click on like I don't get a pop up. Can you provide a video or screenshots of what you are seeing. Thanks.
The upper image shows Customer info. It only requires a hover and is automatically dismissed.
The lower image shows Likes. It requires a click to view and a click to dismiss the 'modal' dialog.
It would be nice for both to behave as the Customer info does -- just a hover and a read, nothing more.
Thanks.