Omegaplex (Customer) asked a question.
FEATURE REQUEST: EA9 Line Trend Graph Dynamic Axis Range
Are there any plans currently or in the future to implement a dynamic range setting for the Line Trend Graph Axis? I've ran into several projects where not having this option forced me to use other brands.
Any information or just a solid answer on the subject would be greatly appreciated.
+1 @Omegaplex (Customer),
This was also requested on the following thread...
https://community.automationdirect.com/s/question/0D53u000025WjtpCAC/dynamic-y-axis-range-on-line-trend-graph-cmore
Regards,
Garry
Thanks for the feedback. It is important to us. This is a highly requested feature by other customers and us alike. We have passed it on to the developers, but we have no schedule for when this feature would be implemented.
A really messy workaround I have done is multiple line trends on top of each other with different ranges. The proper chart is displayed based on the selection for the ranges. This only really practically works for simple projects. In one case I have various zones that temp and humidity are monitored. The temp sits around 35-45 all day and they like to see it more precise normally but sometimes it is useful to correlate it with the ambient temps requiring a new scale on that axis. A PB above allows that selection and triggers a new screen.
Again it's messy but so are a lot of my C-more workarounds.
Trend Graphs in C-more could benefit from a number of improvements that have been a long time coming. Variable Y axis, variable X axis, date/time picker, accuracy improvements, log booleans.