BobbyS (Customer) asked a question.July 22, 2021 at 5:45 AMWill the BRX Sim work with high speed timers/counters?Expand PostDo-more/BRX
Garry (Customer)5 years agoHi @BobbyS (Customer),The Do-More Simulator will not work with the High-Speed Input Functions. This is dependant on the model that you are working on. The simulator is usually just for testing.Main menu | PLC | System Configuration... Select IORegards,Garryhttps://accautomation.ca/series/brx-do-more-plc/ Expand Post
Hi @BobbyS (Customer),
The Do-More Simulator will not work with the High-Speed Input Functions.
This is dependant on the model that you are working on. The simulator is usually just for testing.
Main menu | PLC | System Configuration... Select IO
Regards,
Garry
https://accautomation.ca/series/brx-do-more-plc/
Thank You!