ADC_AutomationControls_PE02 (AutomationDirect) asked a question.
Productivity Suite 3.9.1 Release
Productivity Suite 3.9.1 Release
Notes: This version includes a security update. A stop-mode transfer will be required when updating from a previous version.
We are pleased to announce the release of Productivity Suite 3.9.1 featuring:
- An updated CA certificate for new Google TLS certificates used for EMAL instruction
Several bug fixes:
- GUI not enforcing a Stop Mode transfer when project created in a previous version of GUI that included STMR instructions. A Run Mode transfer results in critical error E04312
- Deleting a Bit-of-word tag that is used in a Data View, then saving the project can corrupt the Project file
- If an invalid tagname is entered in a Data View and the Data View is closed before clicking out of the field, the GUI generates errors when opening the Data View again
- GUI not allowing Find Home command to select GPIO input 1 to Switch 1 definition if other GPIO point previously selected
Productivity Suite 3.9.1 Release