MoiGonzaga (Customer) asked a question.
Hello, community,
I currently have a CR1100 scanner connected to our software application in order to read QR Codes in our daily activities. In order to work properly between the software app and the scanner we need to configure the device with the following commands:
- A4: Reset RS 232
- E4
- E3
- A3
- B2, and
- D4
So, I need to scan 6 different QR codes. Is there a way that I could take the commands of each of those 6 codes and put them in a single QR Code? (My idea is to take the 6 different commands and create my own QR Code)
In that way, anytime that a new cr1100 arrives and needs configuration instead of scanning 6 times I will just do it once.
I will appreciate any comment or guidance.
Regards,
Moi Gonzaga
MoiGonzaga,
Yes there is a tool called Cortextools2. This is some software that was created by Code. You can download the software here. https://codecorp.com/products/code-reader-1100. Select “software” then navigate to CortexTools2.
The barcode generated has all of the configurations you selected.
I hope this helps.