andrewswf (Customer) asked a question.

Modbus Addressing in Ignition

Anyone familiar with modbus addressings in Ignition from inductive automation. I have directlogx 06 plc. set the ip and can connect via modbus tcp driver. But no address im using wants to connect/display?

 

Thank you in advance.


    • andrewswf (Customer)

      Tech support had me download the sheet. But I'm still not having any luck. I can ping the PLC with success. But for someone the modbus address doesn't seem to work. I was hoping to find someone with Ignition specific experience as i feel maybe its on that end I need to change something

  • kewakl (Customer)

    I have no Ignition experience nor DL modbus address experience, but....

    What mode are you using? Pg4-12 and pg4-13 of the DL manual that Garry linked will most likely help you in determining the Modbus addresses of the DL06 address space.

    There is a link inside the Ignition doc that Garry linked.

    That link is https://docs.inductiveautomation.com/display/DOC80/Modbus+Address+Mapping

    This doc deals with the perceived oddities of the DL's octal address space. (it references DL240, but ht eDL06 is octal as well.)

     

    hth

    Expand Post
  • AkaHammer (Customer)

    • What Gary said plus I used this tool from Automation Direct under support downloads utilities it is called Modbus TCP Master Program. For use in troubleshooting Modbus TCP connections to Modbus TCP slave devices. Awesome tool, it was a life saver when I setup first time Modbus with DL-06 for read and writes to Eurotherm Temp controllers

     

    • andrewswf (Customer)

      I can connect, but im not really sure what im looking at. whether i put in 102 for the coil and 3139 for the modbus address the screen looks the same.

  • andrewswf (Customer)

    So, i can connect, read and write via modbus tcp master program. But it does timeout on me after a few seconds.