kewakl (Customer) asked a question.

Win10 (V3.8.0.14 and 3.9.0.26 act like 1.7.11) GUI does not show *certain* rungs with array elements

Win10, FW 1.2.7.66 SW V3.9.0.26 and V3.8.0.14

Rungs (around) 240 fail to show in editor when Monitor mode is on -- much like happened in V1.7.1.1

see PAC Suite V2.4.2.2 Release notes 2.) Monitor mode causes GUI to lock up when an array index is out of range.

Note the mouse clicks on the 'scroll-up' and 'scroll-down' arrows of scrollbar

 

Once this issue is triggered, I must restart the software to see these rungs again.

If I disable the offending rungs, the rungs show in monitor mode -- except if I have triggered this issue

I tried breaking the multiple branch rung into separate rungs, issue still manifests, so it does not appear to be related to rung configuration

This is a relatively new issue to this project. I do not think that V1.7.1.1 was used at any point in this project's development.


  • ADC Community_02 (Automationdirect.com)

    Best option would be to be online with the CPU and create a system report and then use the contact support form to send in so it can get sent over to our development team to review.

    • kewakl (Customer)

      Thanks. I had planned to do that, but frustration crept in. I had to take a break.

      When I get back to the crashcart, I will get a sysrep.

      I don't have the forum account creds on that laptop, so it may take some time.