Robbo (Customer) asked a question.
Is it possible to feed a gyro / compass signal into the PLC
Hi Everyone. Is it possible to feed a gyro / compass signal into the PLC via RS 232 or ethernet and then use that signal for PID to control a pwm output to some electric motors? For instance 4 electric motors controlling some wheels on a robot. You lock a set heading from the compass and the motors will keep it going on that heading ?
Thanks in advance
Paul
I don't see why not but if you're going to be doing anything high level I would look more into using an Arduino or other microcontroller.
Hi Adisharr, thanks for the reply. I looked at Arduino options options but Coding is in no way my strong point. Im pretty happy with ladder and its something I'm hoping to do myself with a bit of help. If i went down the Arduino route i think i will be trying for years to come.
RS232? How fast does response time need to be?
Hi Todd, as fast as possible if its stable. I would be looking to have the baud rate at 115200 for the RS232. But. if its possible im happy for it to be slower just to try it all out.
What PLC were you planning to use? Some controllers are better with ASCII communication through the serial ports.
Do you have a part number of the gyro/compass so we can see the protocol?
Regards,
Garry
Hi Garry. I was hoping to use a click brand to keep the cost down and associated software, but I’m also looking into using codesys so I can use anything really.
I have a habit of running before I can walk so I may start on simple project first. Get used to everything then move on. My main thing is I wanted something I could expand on so I wasn’t buying twice.
here’s a link to the gyro compass for info. https://aositilt.com/compass/e1/
all the best
Paul
The specs on that seem to say 10 readings per second, so RS232 will be fast enough. I havent used RS232 in a long time, but from what I remember you can get something like 15 reads per second out of good systems, so the PLC shouldn't be a bottleneck here ith the device only allowing up to 10 reads per second (100ms rate)
Hi Paul,
It looks doable with the Click PLC after reviewing the manual.
https://aositilt.com/wp-content/uploads/2018/02/MANUAL-APPCOMP3A-360-with-LOGGING.pdf
Here is a post that I did with the Click PLC and ASCII to the Solo Temperature controller.
https://accautomation.ca/click-plc-modbus-ascii-protocol/
This will give you an idea of the programming involved on the Click PLC side.
You may also want to consider using a Productivity 1000 unit. This is comparable to the Click pricing but will handle ASCII code better.
https://accautomation.ca/productivity-1000-series-plc-modbus-ascii-protocol/
This will give you an idea of the programming involved in using the P1000 controller on the same application.
I hope this helps you out.
Regards,
Garry
Hi Garry,
Thank you for the advise and links. Ill have a good read through them and hopefully get something started.
No Problem Robbo.
Let me know if you have any questions.
Regards,
Garry
https://accautomation.ca/series/click-plc/
https://accautomation.ca/series/productivity-1000-plc/