golightlyj (Customer) asked a question.

EA9 Monitor connect to 5370 CompactLogix Controller

Hello,

 

I am new to C-More and setting up a system with a 5370 CompactLogix Controller and a EA9-T10WCL Monitor. I was under the impression given all the communications options that communication to a PLC via ethernet was possible. When I looked at the instruction manual the only cables listed that connect to a CompactLogix is an RS-232 cable pn: EA-SLC-232-CBL. I do not have an RS-232 port on my PLC. Can I communicate directly with the PLC? I found these EDS files but none of them directly say AB CompactLogix ...

 

Please Help!


ADC_HMI_PE likes this.