mdjames (Customer) asked a question.
Hi There-
This is my first ladder logic program so I was hoping to get some experienced eyes on it to see if I'm on the right track, or if I'm missing something.
What I'm essentially aiming for is to monitor two analog sensors, and activate output pins based when those sensors exceed a threshold for a certain amount of time.
More specifically, the sensors are current sensors. When either current sensor exceeds a set value (270A in this case) for 5 continuous seconds, it should trigger Y001. When either current sensor exceeds the set value for 15 continuous seconds, it should trigger Y002.
I'm mostly concerned I might be missing an interaction between the timers. Will they operate independently and in parallel?
Below is a screenshot of my logic. DF1 is the value of current sensor 1, DF2 is the value of current sensor 2.
Edit: I'm planning on using a single Click analog PLC.
Thanks!
Your code looks good. The timers act independently.
The only thing that I see is if DF1 exceeds the threshold and after 3 seconds, DF2 exceeds the threshold the timer keeps timing. After 4 seconds DF1 is below but DF2 is still there to make the timer expire and turn on the output. Your program is a combination of both DF1 and DF2.
If this is not desirable, then just use separate timers for each condition and parallel the contacts on the output.
Regards,
Garry
https://accautomation.ca/series/click-plc/