rixtoy59 (Customer) asked a question.
Does any one know if the Productivity suite actually drives the ethernet connection while in simulation mode? If so what address does it use? The one from compiled program or just the system (127.0.0.1) I was able to simulate a M340 and Maple touch screen
and test the combined results. Would like to do the same with p2000 and C-more.
look at help topic P308 for limitations of simulator.
Yes, you should be able to have the PAC simulator talk with the HMI. HMI needs to point to the IP of the PC that is running the simulator.
Maybe I didn't explain properly. With unity and Maple I was able to run both PLC sim and HMI sim and have them interact. I was attempting to do the same with C-more and Productivity.
No. The CMore simulator is lonely in a universe by itself!
Sorry for any confusion.
No worries thanks for the reply.