Wyatt (Customer) asked a question.

I am new to modbus addressing and communication. I am using a CLICK C0-10ARE and have been asked for the modbus register map. Does this just get set up using the SEND and RECIEVE commands in the PLC software?

The way I somewhat understand it is that you pick your CLICK addresses and tell them which MODBUS addresses you want them to coincide with. Any and all information is welcome including a good place to look for knowledge on this type of communication.

 

 


    • Wyatt (Customer)

      Thank you Garry. Both of these were a big help.

       

      • Garry (Customer)

        No problem Wyatt.

        The one thing that is sometimes confusing is the terminology with Modbus.

        Modbus is a master/slave type of protocol. The slave will not do anything until the master instructs the slave.

        Modbus TCP is an Ethernet Connection - The master is also called a Client and the slave is called a Server. Multiple masters are possible on this network.

        Modbus RTU or Modbus ASCII is a serial connection. (RS232, RS485, etc.) You can have only one master on this network.

        Here is a good video explaining the actual information being passed on this protocol.

        https://www.youtube.com/watch?v=OvRD2UvrHjE

        Let me know if you have any questions.

        Garry

         

        Expand Post