asikyle (Customer) asked a question.
We're looking at a EPCOS - TDK Electronics NTC 10k 3988k bead thermistor (B57861S0103A039) for use with the P1-04NTC, and a little confused about the configuration of the P1-04NTC. There seems to be two options for 10k, either Type 2 or Type 3.
Are there recommended probes that fits these type curves precisely, or are otherwise just the typically recommended probes to use with the P1-04NTC?
Is there a way to configure the module with the constants given by the manufacturer, if they're available?
Is there something specific we can look for when trying to decide if the TDK probe (B57861S0103A039) will work well (or not at all) with the P1-04NTC?
Thank you, any guidance is greatly appreciated!
Take a look at the attached NTC MODULE R/T CHART to see if this answers your question.