Elias20 (Customer) asked a question.
I'm having trouble connecting to the BRX simulator on domore 2.8
Once I downloaded and installed domore 2.8, the first time I started the simulator it worked perfectly for me, after closing the program, moments later I reopened domore 2.8 and wanted to reopen the simulator, the simulator window appears, but in the domore program tells me that it has not been possible to connect to the simulator, I uninstalled and reinstalled but it keeps telling me that it is impossible to connect with the simulator, but if I use domore 2.7 I can use the simulator perfectly, so if someone happens the same and You have the solution, could you please share it with me.
Hi Elias20,
The software is working well for me. I'm running Windows 10 64-Bit machine.
What are you running it on?
Regards,
Garry
https://accautomation.ca/series/brx-do-more-plc/
FYI, each version of Designer comes with its own Do-more Technology Version-ed Simulator.
Hence, if you launch the 2.8 Simulator, but do not shut it down, if you later run 2.7 Designer, it will NOT be able to connect to the "2.8" Simulator that is currently running (only one version of the Simulator can run at a time).
Not sure if this is what you are seeing.
You might also try rebooting just in case the Comm Server is hung - that can affect connecting to any PLC.