Garry (Customer) asked a question.
I am trying to communicate Modbus TCP from a C-More Micro to the Productivity Suite Simulator and receiving the following error code:
P499:Recv.ErrCode0090
This code is not listed for the productivity PAC, but it is for the AB driver and says:
Remote node cannot buffer command.
Communication works when I use the Productivity Ethernet Driver, but I want to use the Modbus Driver so additional equipment can be tested.
Thank you,
Garry

Thank you for the follow up!
I have been able now to communicate with Factory IO.
The issue was within Factory IO and assigning the Modbus inputs and outputs.
Here is the configuration of the Factory IO Modbus TCP/IP Client.
Thanks again for the assistance.
Garry
https://accautomation.ca/series/productivity-1000-plc/