kman63 (Customer) asked a question.
How to change the count direction of STP-DRV-4850 and a Homing issue
I am using a p1000 with SCL to control the driver. I cant seem to Find an SCL command to reverse the count.
also I am having an issue with homing. I have set the DL1 and then use SH3L. The motor goes to the home switch and stops. But it does not change the drives count to 0.
For setting the encoder counts back to zero after a homing move. Look at page 48 of the SCL manual:
https://cdn.automationdirect.com/static/manuals/surestepmanual/scl_manual.pdf
" For example, to set the position to zero after a homing routine, send EP0 then SP0."
For reversing the count page 44 of the SCL manual:
Ah yeah I overlooked this one. Thank you, that should definitely work.