RobotArm (Customer) asked a question.

Should I use door interlock enabling and safety relay enabling to create the machine status flags?

For example, I want to monitor the safety relay.

Should I connect 33 to 24V+ and connect 34 to PLC digital input ?

My plan is that if the machine is fine, then 24V+ should be detect by PLC digital input (High), then my PLC will know the status.

 

Capture2


  • Todd Dice (Customer)

    I do the same. I also use the second set of contacts, 13 to +24V ,14 to PLC output module V+ common, to any pneumatic, motorized, etc. operated system the light curtain is guarding.

     

    As an example, a machine I built required the operator place trays into a motorized down stacking feeder. Operation required the ability to load trays while machine remains in operation. Light curtain disabled operation of the down stacker once blocked. I had the light curtain relay auto start, so once unblocked, timer in PLC had to time out before down stacker would resume.

    Expand Post