Marco (Customer) asked a question.
I am going to buy a sinking PLC (1st picture).
I will need to buy a sourcing sensor (PNP sensor, 2nd picture) to use in this PLC.
I will connect 24V to brown wire of the sensor, 0V to the blue wire of the sensor.
I will connect the black wire of the sensor to X1 of the PLC. AND I will connect 24V to C1
Is any of my understanding incorrect??
The Inputs can be sinking or sourcing.
With the sensor shown you would connect:
24 V+ > Brown wire of the sensor
24V - > Blue wire of the sensor & C1 on PLC
Black wire of the sensor >X1 on PLC
See attached pdf from chapter 3 of the Click manual that details sinking/sourcing wiring for inputs and outputs.