GeniusInTraining (Customer) asked a question.
Hello Everyone, I have been reading about Pointers, Loops and indexing but not sure if thats what I want or need.
I need to store some data, some will be time duration values and other will be real time integers, this will be triggered by events, when the event happens I need to move/copy my data to a register until the next event happens and then store it without writing over the last data and to a new register location at the end of the shift we will clear all data and start over
Example when x happens, I started a timer T1 and at the end of x I copy TD1 to DS500, then the next time the event happens I need to copy TD1 to DS501
My friend did a block copy with a index and it worked but that wrote over DS500, I need that but not to write over the old data
Thank you
Mark
Have not run on an actual Click, but it works in my head. :-)
Store TD1 to DS500 and up
Thanks Todd! I will give it a try
One thing I would change is the copy command that places 500 into DS499. It should perform it via a N.O. one-shot at the start of your shift, rather than at end of shift.
And, I forgot the END statement! Eek!
Updated and confirmed it works via my desktop Click in the office.
Store TD1 to DS500 and up